This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于AFE4403、AFE4404的应用问题

Other Parts Discussed in Thread: AFE4403, AFE4404, AFE4400, AFE4490

       最近有一个新的项目,是做一个穿戴式的医疗设备,有点类似于健康手环。之前参考过一个37度手环的案例,关于TI的模拟前端(AFE),不知道有没有对这方面熟悉的工程师?现在需要技术支持,做选型方案。主要是两个方面:一个是人体体温测量(TI可参考的比较多TMP系列、LM系列),另一个类似于脉动式血氧计AFE4403,但不是测量血氧与脉搏,也是利用集成AFE加上光源、探测器,用于测量胆红素。
       我在TI的AFE查找了一下,大部分是测量ECG的比较多,只有少数几款像AFE4400、AFE4490、AFE4403、AFE4404,适用于测量血氧、脉搏,集成的AFE前端只需要接相应波长的LED、光电探测器,就可以工作了。现在这个项目原理大致是这样的,采用红光、绿光两个不同波长的光,照射皮肤,因为波长不一样,透过皮肤发生反射的深度不一样,通过反射光,测量血液内的胆红素浓度,胆红素浓度越高,皮肤表面呈现黄色越深,就是我们常说的黄疸。
       我的问题主要是这样的,我们这样的项目,是否可以采用AFE4403、AFE4404,因为集成的AFE需要的外围电路少,可靠性高,集成度高,体积小是做穿戴式理想的方案;AFE4403、AFE4404是否专门用于测量血氧、脉搏,如果更换不同的LED、探测器,是否可以达到我们的项目需求?我也大致看过PDF,但是很不确定。