This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC16DV160HFEB: ADC16DV160HFEB

Part Number: ADC16DV160HFEB
Other Parts Discussed in Thread: WAVEVISION5, ADC16DV160

Hello, two weeks ago I was able to use this board normally, but now when I open the WaveVision5 software, an error message pops up. Even though I followed its instructions, the error persists, and I could use it just fine two weeks ago. Additionally, when powering the ADC16DV160, it heats up excessively, and a 3V input voltage corresponds to a current of around 4A. I would really appreciate your help. Thank you.