This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1291: DRDY位输出异常

Part Number: ADS1291

工程师你好,我在使用ADS1291时,给他上电然后初始化后,首先测试了Vref=2.4V,VCAP1=1.2V和VCAP2=5.2V,一切正常;然后在测试DRDY时,发现脉冲是向下的,频率是500HZ,如图所示:

然后我怀疑是SCLK的问题,并测试了SCLK的输出,发现如图所示(两个图都是),频率是1MHz,你看是这部分的原因吗?

此外,我通过设置寄存器,将ADS1291的内部时钟输出出来观察,是标准的512KHz,没有问题。

基于此,目前遇到的问题是DRDY位的频率输出正常,但是波形不正常,怀疑可能是SCLK的原因,请问是什么原因造成的呢?

期待您的解答!