This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL0102-100: TPL0102-100 输出问题

Part Number: TPL0102-100


您好,我们的需求是通过电位器配置DCDC的FB电阻,让电压可调。 不过我们的DCDC做了负压输出的配置。上电后发现DCDC输出不正常。状况如下:

1,电位器及8771同时供电,输出0.3V左右
2,8771先供电,然后电位器在供电,输出负压正常,然后配置电位器,但是输出不变。
3,电位器先供电,然后8771在供电,输出负压正常,然后配置电位器,但是输出不变。


 这种BUCK配置成负压输出,然后通过电位器调节的方案可行嘛。为了匹配这个负电压,我们特意把电位器参考到了-5V上。这样是否妥当?

另外我想问一下,如果在电位器的抽头端和高端(或者低端)连接万用表,然后配置电位器,可以测量出电阻变化嘛?电位器输出是电压还是纯电阻?