This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电平转换芯片74CBTD3384的用法



大家好,我最近想自己动手做一块dsp_f28335,在电平转换芯片的选择的时候有些疑惑,求助大家,谢谢。

参考相关资料,dsp引脚3.3V,qep信号输入为5V,所以想在这之间加一个74CBTD3384,他是一个双向的信号传输,qep的5V信号经过74CBTD3384后变成3.3V的信号,进入dsp的管脚,这一点我可以理解;但是如果,我将一个3.3V的信号和一个0-3.3的方波信号通过74CBTD3384后,他出来后是什么样子呢,还是0-3.3V的电压还是变成了0-5V的方波信号?

我将一个0V信号通过它,出来后还是0V信号吗