This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

数据转换芯片的数据有效输出信号(DVALID)问题



正在研究和使用TI DDC112U这款芯片,它所需的时钟CLK和转换控制信号CONV均由FPGA产生,CLK频率为10MHz,CONV频率为1000Hz,用示波器观察到CONV信号的高低电平切换时与CLK的上升沿同步在1纳秒左右。由于CONV信号一个周期内的高低电平持续时间都是500us,所以芯片应该是工作在Continuous Mode下。

但是每次重新加载FPGA程序以后,这款芯片的数据有效输出信号(/DVALID)有时一直为高,有时如果输出为高的话,用示波器的探针点一下PCB上/DVALID信号经过的一个过孔,DDC112U的/DVALID就能给出低电平了。

为什么会出现这种工作不稳定的现象,请问有哪些原因可能导致这种现象?