Part Number: ADS52J90
我使用ADS52J90进行16通道设计时,SPI可以正常通信(例如将SDOUT管脚牵出来可以用示波器看到SDOUT波形),寄存器配置0Ah为3000h,2h-5h无论是default还是custom的配置,DCLK、FCLK和16对数据差分对OUTP/M都不能用示波器测到,感觉像是AD没有正常工作,后面的寄存器也按照default配置,或全为0的配置。我采用的是LVDS,16bit,14位ADC,系统时钟10Mhz。总之不知道应该怎么解决这个问题,无法得到DCLK、FCLK和数据,以进行下一步设计,请帮我提出一点建议,谢谢!