This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1293输入共模电压的问题

Other Parts Discussed in Thread: ADS1293

(1)因为法规要求,需要给ADS1293的各导联输入口加上10V有效值的共模50hz工频电压,而ADs1293内置最大输入为VCC,也就是3.3V,如何才能接入10V有效值的共模电压?

(2)心电各导联的参考地是什么?如果接浮地的设备也应该有一个参考的吧

以上请帮忙解答下,急用,谢谢

  • 什么法规这样规定的?

    感觉 ADS1293 的数据手册规定

    CMVR Common-Mode Voltage Range TMIN ≤ TA ≤ TMAX                      0.5 ~ VDD – 0.5 V

    不允许加上10V有效值的共模50hz工频电压