This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS324+IMX185 图像闪烁



SN65LVDS324+IMX185+ISP,SONY LVDS parallel 12-bit  1080P30,寄存器0x09: 0x21 ,0x0a:0x61,图像一直有闪烁现象,不规律,主要是色彩有变化,图像形状没有改变,使用SN65LVDS324测试模式,输出彩条依然有闪烁现象,测试CLKOUT:74.25MHz,VS:30Hz,HS:33.78KHz。更换SENSOR,使用MN34229+SN65LVDS324+ISP,2 CHANNEL 2 PORT 12-bit 1080P30,寄存器0x09: 0x02 ,0x0a:0x61,图像也有闪烁现象。哪位高手知道如何解决,或者怎么排除这个问题是否与SN65LVDS324有关,谢谢!