Other Parts Discussed in Thread: ADS62P19
Dear TI专家:
您好。关于ADS62P19模拟输入驱动电路我有些疑问,还请指教。
在我的系统中输入ADC的信号频率范围从1MHz-100MHz,从Figure 45和Figure 46中可以看出在频率小于100MHz时,电阻大于3K欧姆并随着频率的降低而呈指数形式增加,电容在该频率范围内基本维持在3.5pF大小不变。由于电阻与电容是并联的关系,故基本可以认为ADC的输入电阻就是电容的阻抗,1MHz时是45.7K欧姆,100MHz时是457欧姆。
再看下面驱动电路图纸,靠近输入口位置,两个25欧姆的电阻串接后并在输入口,该接法直接导致ADC的输入阻抗降低到小于50欧姆的水平。
问题:
1、这里为什么要这样做呢?是为了与假设内阻为50欧姆的信号源做阻抗匹配吗?如果是这样的话,为什么在两个25欧姆后面还要并接两个 50欧姆的电阻呢?22pF的电容我理解为与L形成低通滤波器。
2、我的信号源是差分输出模式,那么是否可以不要驱动电路中的两个变压器,直接将我的信号源接到figure47中第2个变压器右侧线圈处?
3、我的信号源是VGA输出的差分信号,信号源差分内阻为150欧姆,驱动电路该做些什么样的变化?是否有必要再插入抗混叠滤波器??
期盼您的回复。感谢!