Part Number: ADS8568
最近项目中使用到ADS8568芯片,使用串行接口,硬件控制,当给convst信号后,8路模拟都有-2.5V电压。能读取,其他一切正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
当给convst信号后,8路模拟都有-2.5V电压。
是说CHXX的输入电压吗? 请详细说明一下具体问题。
ADS85x8 12-, 14-, and 16-Bit, 8-Channel, Simultaneous Sampling ADCs datasheet (Rev. C)
您好,
采样时有-2.5V的偏置电压,这个-2.5V时ADS8568芯片产生的。
这是ADC输入管脚实测的电压?请问输入是悬空状态还是在有输入信号的情况下?
ADS85x8 12-, 14-, and 16-Bit, 8-Channel, Simultaneous Sampling ADCs datasheet (Rev. C)