Part Number: ADS131M02
你好,我正在使用ADS131M02开发一款产品,按照官方提供的驱动进行了修改,在adcStartup()函数中我配置了CLOCK以及GAIN1寄存器,然后调用之后,我读取了寄存器的值,与我写入的值是一致的,但是当我在调用读取131采样数据的函数requestData()时,发现所有的寄存器又恢复了默认值,在这中间的时间段并没有复位131的操作,不清楚到底是什么原因,希望能提供一些思路。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
当您在使用ADS131M02这款ADC(模数转换器)时,遇到寄存器值在调用某个函数后恢复到默认值的问题,这通常可能是由于几种原因造成的。以下是一些可能的原因和排查思路:
硬件复位或电源问题:
requestData()函数期间,硬件电路没有发生任何复位操作,包括上电复位、看门狗复位或外部复位信号。软件复位或初始化问题:
adcStartup()函数只在系统启动时调用一次,而不是在每次需要读取数据时都被调用。寄存器写入确认:
SPI/I2C通信问题:
中断或DMA干扰:
requestData()调用期间干扰ADC的寄存器状态。固件或驱动问题:
硬件连接问题:
调试和诊断:
requestData()调用前后添加断点或日志输出,以观察寄存器值的变化情况。