Other Parts Discussed in Thread: OPA2350
与存在问题部分相关电路如图所示,从BNC接口输入信号本身的频率很低,由于采样要求高阻,并联1M欧电阻,BNC的负端用1.024V基准接。CH1CH2两通道共用一片OPA2350(该芯片带宽远超过实际需求,主要考虑是轨到轨特性,以及公司现有的存货)。由于信号存在一定的工频干扰,加一级RC滤波进行滤除,R=100K,C=0.1uF。截止频率约在15.9Hz。板子本身引入的噪声大约在±0.2mV。当两个通道均接固定的电压输入时(如干电池),系统运行良好,两个通道的误差均在合理的范围内。但当一个通道的电压变化时,另一个通道的电压也会发生相应的变化。如图2为一次采集过程的通道一通道二电压变化图。通道2接的是固定的干电池,万用表测得电压为1.5832V,而通道1接一可变的电压源(DAC)。当通道1保持不变时,如0-2s,18-22s等,通道2也基本维持不变。但当通道1发生改变时,通道2也发生相应微小的变化。通道1变动1V,通道2变动有1mV左右,且两者趋势大体一致。将通道1和通道2调换,即通道1接固定电压,通道2接可变的电压,同样存在这样的影响。
请问这种影响可能是什么原因造成的?ADC、前端运放还是其他的电路部分?ADC的采样率为10k。波形为上位机软件根据ADC的值获得。