This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1255: 使用FPGA控制转换数据的时候drdy信号一直持续为高电平,无法输出数据

Part Number: ADS1255


由于使用的是网上购买的数据转换模块,因此不清楚具体连接方式,我分别尝试过一下几种方式:

1.直接输出WAKEUP指令;

2.按顺序输出SYNC、WAKEUP、RDATAC/RDATA指令;

3.按顺序输出WRREG、SYNC、WAKEUP、RDATAC/RDATA指令;

4.先输出STANDBY、再输出WAKEUP指令;

5.直接用RREG指令尝试读取寄存器值;

在上面的几种操作中,CS信号都是与输出指令同步拉低,D0/D1都为0,CLK信号是一直持续输出,而DRDY都没拉低。请问一下是不是控制方式或者时序出了问题,以及以下问题:

1.想要实现控制的话应该怎么输出控制指令;

2.CS必须在要转换的时候拉低还是可以一直拉低;

3.D0/D1两个信号的作用是什么;