Part Number: ADS131A02
Other Parts Discussed in Thread: ADS131A04
我现在使用ADS131A02做64K采样率的数据采集。我看网上都是使用异步中断从模式来使用这个芯片的,但是64K的中断频率对于MCU来说太频繁了。我看手册里面提到了支持同步主机模式。我有几个问题:1、是不是可以把ADS131A02当作SPI的主机,AD数据转换完以后自动输出AD数据到做SPI从机的MCU上面去,这样MCU那不就可以使用DMA在后台搬运数据,不用产生中断;2、如果第一种可以实现,那么在ADS131A02启动过程中如何来配置寄存器,这时ADS131A02做主机,MCU做从机,MCU无法主动向ADS131A02发送数据。
我看了您的意思应该是9.5.2.2这一节讲的是同步主模式的通信,这里面的意思就是数据准备好DRDY拉低,开始输出数据,但是我主要是想知道这副图里面描述的芯片初始化配置怎么来实现,因为在同步主模式下,MCU做从机,没办法主动给AD芯片这边发送数据,那么初始化过程中这些寄存器的配置要如何实现。