小弟最近需要做一个项目,包括40个通道的高精度电流采样,技术指标如下:
1.测量范围:0-500mA;
2.测量精度:最大绝对误差:0.01mA;
3.可承受短时间最大电流:5A持续时间1s。
请各位帮帮忙给出一个参考方案,或者ad选型,谢谢各位喽!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
小弟最近需要做一个项目,包括40个通道的高精度电流采样,技术指标如下:
1.测量范围:0-500mA;
2.测量精度:最大绝对误差:0.01mA;
3.可承受短时间最大电流:5A持续时间1s。
请各位帮帮忙给出一个参考方案,或者ad选型,谢谢各位喽!
假设满量程500mA,误差0.01mA的话就已经是超过4位半低于5位半精度的测量了,这个需要从系统信号链调理的角度整体考虑,影响的因素太多了。可先试着考虑下面的内容
1、电流变换的方式。电阻?CT?
2、放大器调理。仪表放大器?精密放大器?
3、ADC。ADC类型?采样速率多少?满量程电压?分辨率?有效位数?INL?DNL?
4、基准。ADC匹配?稳定性?
5、保护。过量程分流保护?保护电路漏电?ESD?
6、测量方式。AutoZero?
7、电源。系统电源轨是多少?DC-DC?LDO?
回答好上面的问题,估计电路的雏形就该差不多了。
希望对你有帮助。
20ppm还好的,ADC可以解决的,不需要像万用表一样多重积分的;不要被吓到
关键难点在于你要多少内阻和多高电压;电流噪声的敏感程度决定你的采样率
这样问是没有办法给出具体型号的