This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS805E输入端悬空有电压的问题



1、ADS805E使用0~5V单端采集的接法,前端接模拟开关。

2、芯片工作、采样数据都没问题。

3、对于悬空的模拟开关输入端采集到电压1.85V。

4、断开AD与模拟开关的电阻47欧,这一电压1.85V来自ADS805E。

5、进一步排查,只要ADS805E能识别到有效的CLK信号,输入端就会有1.85V,否则(无论CLK是常高或常低)都不会有电压。

6、时钟频率为1MHz,降到100kHz,仍有电压,为1.65V。

7、改变CLK幅值2.7V~5V,不会影响电压的有无。

8、输入端接1M欧电阻,仍无改观,要接10k可消除,显然采集阻抗匹配不允许。

问是否有办法消除这个电压,因为被采对象输出阻抗比较大,不供电时希望采到0,否则无法判断它的供电情况等重要参数