This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: 外部加上拉,开漏信号电平转换

Part Number: TXB0104


TXB0104不能用于开漏信号转换,如果A端口和B端口外部分别加上拉电阻,是否就可以进行I2C类信号电平转换?如果不行,原因是什么?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 使用TXB0104 进行I2C信号电平转换通常是不推荐的,因为I2C信号使用开漏输出。
    TXB0104 的工作原理依赖于输入端处于驱动状态时先有足够的电流流入其结构中,以便正常工作。具体来说:
    TXB0104 并不设计为支持开漏配置。开漏信号在空闲状态(高电平时)没有驱动电流,TXB0104可能无法检测到这个状态,导致信号无法正确转化。
    在只有拉电阻的情况下,如果没有足够的电流流动到TXB0104的输入引脚,输出将无法正常转换到相应的输出逻辑状态。

    The TXB*** is not compatible with open drain drivers, please see the I2C buffers landing page for more suitable option instead

    I2C & I3C level shifters, buffers & hubs product selection | TI.com