This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1232高速采样的问题



电路是按数据表中的推荐电路搭接的,晶振采用推荐的4.***M的,PGA为2倍。原理是用比较法测电阻,恒流源流过基准电阻和被测电阻,AD基准电压采来自基准电阻分压,AD测量输入来自被测电阻分压,使用低速测量时(10次/秒),原始输出字波动已经可以做到10个字以内,但是高速(80次/秒)时测值波动较大,采用4个周期的移动平均滤波后,稳定性增强,一次实测数据出现20分钟的长周期波动,波动幅度在800个字,形状类似锯齿波,另一次试验出现的波动周期更长,波动幅度相差不多。在用电池供电,对整个仪器用金属盒屏蔽后,这种长周期的波动现象消失,请问是什么原因呢?初步分析是因为工频电的干扰引起,按数据表的理解,在低速,标准晶振的状态下,AD可以抑制工频干扰。目前的需求是要把采样速度比低速时提高2到4倍倍左右,应该怎样选择晶振能使得AD在高速采样时也可以具有抑制工频的能力,或者选择低速采样,而使用更高频率的晶振?