This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1305M25输出的单位串行码流形式



码流是否有固定周期呢,例如CLKIN为20MHZ,那么输出的单位码流也是按20MHZ输出的,而码流占空比是变化的。那么这个占空比是体现在单个时钟周期内还是连续多个时钟周期内呢?举个例子如果输出码流是50%的占空比,那么在单个周期内就是0和1状态各占半个周期时间;如果是体现在连续多个周期比如连续8个周期,则意味着0和1各占4个周期时间。简而言之,就是说在时钟周期是20M时,输出码流是在每个时钟周期都发生0,1变化还是在连续几个时钟周期内才发生一次这种变化,能否提供一个具体的波形呢,手册中实在是看不出来,谢谢。