Other Parts Discussed in Thread: ISO3082, SN65HVD1476, SN65HVD75, SN65HVD78, SN65HVD71, ISO35T, ISO15
1 ISO3082我查DS寫VCC1=3.3v, VCC2=5V,請問兩個電壓是否可以都接3.3V?
2 SN65HVD23D我查DS電源電壓寫5V, 請問是否可以用3.3V
3 請問還有沒有其它轉RS485的訊號IC是3.3v?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1 ISO3082我查DS寫VCC1=3.3v, VCC2=5V,請問兩個電壓是否可以都接3.3V?
A:不可以,VCC2的供电电压范围为4.5V~5.5V,最小不能低于4.5V。
2 SN65HVD23D我查DS電源電壓寫5V, 請問是否可以用3.3V
A:也是不可以的呢,SN65HVD23D的供电电压范围也是4.5~5.5V,典型值为5V,所以3.3V不允许。
3.請問還有沒有其它轉RS485的訊號IC是3.3v?
A: 3.3V的很多, SN65HVD75,SN65HVD1476,SN65HVD78,SN65HVD71等。
如果需要带隔离485收发器的,比如ISO35T,ISO15.
請問
看起來好像分SN沒隔離的和ISO有隔離的,對吧?
請問有隔離的是不是抗雜訊比較好?
TI的隔离器件一般都是ISO开头的。
因为通常来说485的应用环境比较复杂,简单来说采用隔离的更能保证通讯正常,信号完整性。