Other Parts Discussed in Thread: CC2541
使用条件:
1、使用内部1.24V基准源;
2、10位精度模式;
3、CC2541采用外部可调数字电源供电,分别从3V、2.9V、2.8V三个档位测量同一个外部稳定电压1V。
现象,测量结果3V供电时时比较接近,随着供电电压降低,测量值不断升高。
数据手册没有给出ADC部分最低的工作电压,但是感觉2.8V应该不会影响测量精度吧?
从转换码上看,感觉像是内部基准源会随外部电源供电变化200mV/V,远大于数据手册的4mV/V。
因为我们的产品最终选择的是3V纽扣电池供电,需要监控纽扣电池的电压判断电量,所以如果ADC测量不准会很麻烦,望各位前辈帮忙看下,可能存在的问题?多谢!