Part Number: ADS4142
Can the ADS4142IRGZ and ADS4149IRGZ be compatible? I have a capture card board that uses the ADS4142IRGZ, and now I want to upgrade the sampling rate. Can I directly replace it with the ADS4149IRGZ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS4142
Can the ADS4142IRGZ and ADS4149IRGZ be compatible? I have a capture card board that uses the ADS4142IRGZ, and now I want to upgrade the sampling rate. Can I directly replace it with the ADS4149IRGZ?
The pin definitions for these two chips are the same, and you need to refer to the data sheet for specific electrical parameters and register configurations.
The capture card board you mentioned has ADS4142IRGZ on it. Is the board from TI or was it designed by yourself?