Other Parts Discussed in Thread: AFE58JD48EVM, AFE58JD48
Dear TI Forum Members,
I have encountered a "timed_out_error" while collecting signals using the AFE58JD48EVM in conjunction with the TSW14J50EVM through the HSDC Pro software. I have three TSW14J50EVM boards at my disposal. When following the same procedure for signal collection, only one of the boards exhibits this issue, while the other two function without any problems.

The figure below shows my hardware connections and the sequence of operations.





However, after multiple attempts of rebooting and repeating the process, the faulty board occasionally functions properly.
The LED lights D1, D3, D6, and D7 are off, while D2 and D4 are blinking, and D5 and D8 are lit.
Could you please provide some guidance on how to resolve this error? Any insights or suggestions would be greatly appreciated.
Best regards,
Feng Tao.