Part Number: ADS124S08
Other Parts Discussed in Thread: ADS1247
我正在使用这个芯片进行PT100的测量,测量电路为SBAA330上的参考电路(为ADS1247/8推荐电路,跟ADS124S08手册略有差异),测试时发现一个奇怪的问题:使用固定电阻代替PT100传感器时,测量数据非常稳定,且值正确,实际接PT100传感器时,如果温度很平稳时,数据也比较稳定,但只要传感器温度变化时,比如手捏住传感器,温度从25左右攀升至30几度过程中,ADC的数据就开始紊乱,采样温度本应在手接触传感器后开始升高的,此时反而会下降,但过几秒钟又会升高,但升高过程并不是平稳的,会突然从一个温度跳动到另外一个温度,中间没有过渡过程。从读到的ADC值也可以明显的观察到这种情况(比如从0x22xxxx直接跳变至0x23xxxx),最后当温度不在变化时,读数也恢复正常,也能显示正确的温度。想问一下这种只能测量稳定的信号,变化的信号就异常的原因,可能是什么。(这个方案设计测量2路PT100,更换通道测量,情况是一样的,另外测试过程中还更换过ADS124S08,也没有改善,看起来好像并不是硬件方面的问题,但是读写芯片是严格按照手册来进行的,读写寄存器什么的都是正常的。另外外部滤波电路采用的是10K/3.3nF/33nF.)