This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5463: The DRY pin output of the ADC is at 250M, and also at 750M, and the harmonics at 750M are quite comparable in size to those at 250M.

Part Number: ADS5463

The clock signal I provide to the ADC is 500M, passed from the LMK, AC coupled, not a standard sine wave, 0.8VP-P. Then I measured the ADC's DRY pin with an oscilloscope and found both a 250MHz and a 750MHz signal, both having similar peak values. Is this normal, due to the need to transmit data on both the rising and falling edges?