Part Number: ADS1220
桥式压力传感器,
供电1.5mA
零点输出:+-2mV(@1.5mA)
满程输出:60~200mV(@1.5mA)
阻抗:2K~5K
工作温度-30℃~100℃
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于桥式压力传感器的信号调节器和发送器。可以参考下面几个芯片:
PGA300 数据表、产品信息和支持 | 德州仪器 TI.com.cn