This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220: 求助压力传感器采集方案选型和应用方案

Part Number: ADS1220


桥式压力传感器,

供电1.5mA

零点输出:+-2mV(@1.5mA)

满程输出:60~200mV(@1.5mA)

阻抗:2K~5K

工作温度-30℃~100℃