小白一个请教专家一些问题
1.我没有pandaboard ,有公司上一代产品可以输出16路1位深度的黑白图像,LightCrafter 4500与公司上一代板子相互链接 除了16路数据通道还需要最基本的那几条线才能实现数据传输。
2. 1位深度速率可以达到4k,如果16路数据进入LightCrafter 4500 之前增加FPGA还能提高速率么?或者说有什么办法提高速率到10k以上?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
只有一个B通道,用10BIT或8BITS.
DLPC350和D4100是完全不同的系统.
另外你是想实现实时传输还是通过片上DDR2/3实现10K以上速度?
现在速度都是片上DD2/3缓寸实现的.
10K通过什么信号源实现传输过来的?
DDR2/DDR3缓冲功能需要开发.当然也可以采用第三方的系统.
如果方便,可以发邮件电话沟通.
按照你的配置最高可以到本2万多HZ.