This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC910: DLPC910+VC707+DLP6500

Part Number: DLPC910

The case number of the closed support request is CS3093874 
hi,All
I followed the DLPC910 documentation and programmed the bit file to the VC707. The power was applied in the correct sequence. The status feedback from the host computer appears normal, and the indicator light on the DLPC910 seems to be functioning properly (D1 is flashing). However, the DMD display is not updating and remains in its initial state. 
0fb5cb91b5bf3572b24e3387904681d7.jpg
Here is the interface of the host computer. Did I miss something?

Pasted image 20251120141326.png
Does the LED3 being off on the VC707 indicate a system initialization failure? 
Pasted image 20251120144946.png