附件是6张8位的图片,想要通过DLP4500实现100Hz的频率投图,曝光时间是周期时间的一半并且同步触发高速相机采图。
问题一:目前在使用LightCraft4500 GUI软件时只能达到10Hz左右的速度,否则就会出现错位,请问如何设置?能够帮助一下设置一下生成bin文件及ini文件学习一下。
问题二:在Firmware Build选项卡中更换原有的图片时不能讲8位的图片添加进去,显示只能添加24位的图片,请问是怎么回事呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
附件是6张8位的图片,想要通过DLP4500实现100Hz的频率投图,曝光时间是周期时间的一半并且同步触发高速相机采图。
问题一:目前在使用LightCraft4500 GUI软件时只能达到10Hz左右的速度,否则就会出现错位,请问如何设置?能够帮助一下设置一下生成bin文件及ini文件学习一下。
问题二:在Firmware Build选项卡中更换原有的图片时不能讲8位的图片添加进去,显示只能添加24位的图片,请问是怎么回事呢?
1、
DMD内部buffer只有48bit,每次DMD显示时从buffer读取图片内容,在48bit以内能达到显示帧率4225fps@1bit和120fps@8bit,当图片超过48bit时每次从flash载入图片最少需要200ms,所以当然图片较多时快速显示会出现断裂或者错位现象。
附件一直上传失败,我将固件和ini文件上传到百度网盘了:http://pan.baidu.com/s/1i4YXUbN
2、
向固件添加时只支持24bit图片,你可以通过firmware build标签页的Create images将24张1bit图片或者3张8bit等图片合成为24bit图片,然后再添加或者更换。
上述网盘内容含有你的6张图片合成的2张24bit图片,ini文件设置的是每秒显示你的一副8bit位图。