This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC900: Question about DLPC900 J26 external parallel video input

Part Number: DLPC900

Hello TI team,

I am working with the DLPC900 EVM and would like to ask about the J26 external parallel video input interface.

I mainly have two questions:

  1. Is there any existing TI or TI-partner hardware solution that can directly mate with J26 and provide the required parallel RGB video input?
    I would like to know whether there is any already-developed source-side board or module, so that I do not need to design the whole interface from scratch.
  2. If there is no ready-made solution, what is the recommended way to design the source side?
    For example:
  • which document should be the main reference for the J26 parallel RGB input timing,
  • whether an FPGA is the recommended approach,
  • and whether there is any reference design or example for generating the required parallel RGB video source.

My goal is to use a high-speed parallel RGB video source for DLPC900, so I would appreciate any guidance on whether there is an existing solution or how to design one properly.

Thank you very much for your help. I apologize if my questions are too basic, and I would greatly appreciate any guidance you can provide.