This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC120-Q1: DLPC120配置文件中默认Effective Output = 75 %

Part Number: DLPC120-Q1

尊敬的TI工程师你好!

请教一下如果我将DLPC120亮度拉到最大65535或者说RGB占空比给到最大59000,按照配置文件CFG_EVM_RevC_2C653471_20180111_COR_MP_v3.cfg 中的描述,

<Data>
<LDCIndex>0</LDCIndex>
<SEQIndex>0</SEQIndex>
<Mode>CM</Mode>
<Pulses>0</Pulses>
<Attenuation>100</Attenuation>
<Comments>Effective Output = 75 %</Comments>
</Data>

我的实际有效输出是不是只有我设置的亮度值的75%?如果是的话,我能不能将有效输出给到100%呢,我直接在这个配置文件中修改为100%可以吗?我想输出100%该怎么做?

期待您的答复,谢谢!!