This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: DLP3010EVM-LC, can the device still function properly after removing the plastic casing and the light source?

Part Number: DLP3010EVM-LC

我们想把外壳拆掉,然后替换我们自己的光源,是买回来就可以直接用还是?光源是否有外接设备接口,接口协议是否有要求。

We want to remove the outer casing and replace it with our own light source. Can we just use it directly after purchasing or not? Does the light source have an external device interface? And are there any interface protocol requirements?

然后外显想接自己的显示屏或者投影,外显接口有什么要求?电源有什么要求?

Then I want to connect my own display or projector. What are the requirements for the external display interface? And what about the power supply?

以上总共三个问题,大伙有空看到帮忙解答一下。确认之后我就准备购置一套来实验看看。

Out of the three questions above, if anyone has the time, please feel free to answer them. After confirming the answers, I will be ready to purchase a set to conduct an experiment with.
套件链接如下:The link for the evaluation board is as follows:
DLP3010EVM-LC 评估板 | 德州仪器 TI.com.cn 

  • 主板、电源板、光源、外显屏幕总成,应该就这4部分。我想要的是4个部分可以随意插拔更换后组装在一起的。
    The mainboard, power board, light source, and external display assembly - these are the four components. What I want is that these four parts can be easily plugged in, removed, and replaced, and then assembled together.