This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

提供分辨率为1080P光源为405nm蓝紫光芯片的投影设备厂家



大家好,我想问一下现在国内是否有厂家已经推出了标准分辨率为1920x1080,光源采用405nm LED芯片。我们想使用这用的设备进行光固化3D打印。

  • 我们有客户会推出lightcrafter6500的.我们会把联系方式推荐给你的.

  • 已经有了现成的方案了。

    产品型号

    PRO6500UV150

    PRO6500VIS900

    芯片

    DLP 0.65 DMD

    DLP 0.65 DMD

    光源

    405 UV LED

    LED(RGB单色光源可选)

    透射比

    1.56

    1.61

    调焦范围(mm)

    约20

    500

    对比度

    1000:1

    1000:1

    默认输出能量

    2800mW

    380lm

    尺寸(mm)

    290*172*129

    310*173*129

    均匀性(JBMA)

    95%

    95%

    偏轴

    0%

    0%或100%

    投影精度

    50μm

    0.5~2m

    投射距离

    150mm

    水平±15.9、垂直±9.08º

    /

    投影幅面(mm)96*54

    景深30mm

    畸变

    <0.1%

    <0.6%

    应用领域

    3D打印

    三维测量