This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP投影如何进行HDMI信号检测



我想咨询一下DLP投影仪的HDMI信号检测是如何实现的。

现在的投影仪在切换到HDMI信道后,没有HDMI信号时会显示一个厂家logo,有HDMI信号后会立刻切换到HDMI信号视频显示。当HDMI信号消失后会立刻切换回logo。

如果我想实现HDMI没有信号时黑屏,HDMI信号出现后显示视频内容,HDMI信号消失后回到黑屏状态。这个功能应该在DLP驱动处实现还是在HDMI解码处实现?如何实现?

  • 通常前端的视频处理芯片MCU会实现这个功能。当有HDMI信号输入时,切换input source到外部parallel RGB信源。当MCU没有侦测到外部信号则自动切换回Splash画面,即开机logo,也可以切换到内部测试画面-黑场。所有对投影显示的控制都是前端MCU通过发I2C命令来实现的。