Hello
有个问题想请教大家,我正在画原理图,用到3438+2005,DLPA2005上的LS_OUT脚 作用是什么,2005上1.8V的load switch的作用是什么?DMD和3438的1.8V供电必须由DLPA2005上的 load switch来控制供电吗?可否直接用外部DCDC供电呢,TI的参考文献也看了,好像这一块没讲清楚
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LS_OUT这个脚的作用是做1.8V开关控制,即由外部的DC/DC提供一个1.8V输入给DLPA2005,然后2005在开、关机的时候自动控制1.8V输出给系统。最好不要用外部的DC/DC直接供电,因为DLPC3438在开关机的时候有严格的时序要求。