video 和pattern 分别支持1280*800 和912*1140,这对的吧?那两种模式对投影出来的画面效果有什么区别,或者说为什么要设置两种模式?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
video 和pattern 分别支持1280*800 和912*1140,这对的吧?那两种模式对投影出来的画面效果有什么区别,或者说为什么要设置两种模式?谢谢!
因为这是嵌入的系统, 因此要投影FLASH pattern,就需要设置,触发方式, PATTERN BITS数, 曝光时间, PATTERN序列扥等参数,我们是有基于VS2010的简化系统, 但是是针对特定FLASH Pattern的, 我们可以共享给您,请留下联系方式.
对使用DLP4500所要求的相机和视野,有几点没有理解的地方,希望能得到您的解答,谢谢!
1. 资料图中:为什么相机分辨率*60%得到的才是有效分辨率?
2. 左边图中DLP4500 Field of View的有效分辨率为什么是912*570?
3. 如果按照“相机分辨率要是DMD分辨率的4倍”计算得:912*1140*4=410万,这样要求三维测量系统里的相机至少410万分辨率?