This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP NIRscan EVM评估板相关技术参数

Other Parts Discussed in Thread: DLPNIRSCANEVM

想咨询贵公司DLP NIRscan EVM评估板相关技术参数,主要包括以下几点:

1)波长范围/波数范围

2)波长分辨率/波数分辨率

3)信噪比

4)吸光度重复性/准确性

5)波长重复性/波数重复性

6)波长准确性/波数准确性


  • 参考: http://www.ti.com.cn/tool/cn/dlpnirscanevm

    High Performance EVM MobileSensing EVM
    Key Features DLP NIRscan DLP NIRscan Nano
    Evaluation Module (EVM) Usage Benchtop/Portable Battery
    Featured Digital Micromirror Device DLP4500NIR DLP2010NIR
    Micromirror Array Size (pixels) 912 x 1140 854 x 480
    Micromirror Pixel Pitch (µm) 7.6 5.4
    Micromirror Tilt Angle (degrees) +/-12 +/-17
    EVM Wavelength Range 1350 - 2490 nm 900 - 1700 nm
    EVM Spectral Resolution 12 nm 10 nm
    EVM Max Scan Speed (kHz) 4 2.88
    EVM Signal-to-Noise Ratio 30,000:1
    (transmissive head)
    6,000:1
    (reflective head)