This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500亮度与图像分辨率



请问在Pattern Sequence Mode下,是否可以进行亮度控制,就是控制三个灯的流明数,可以达到时明时暗的效果

还有就是在电脑端制作好的一个912*1140的图片,传到DLP上,在Pattern Sequence Mode下,就会发生形变,请问如何修正这种形变,使投影出来的图片显示正常

谢谢!

  • 亮度可以通过LED, RGB PWM来调整.

    形变有几个原因: DMD旋转了45度, 另外一个是镜头的原因, 和光学的均匀性有关. 针对不同应用,和要求精度的不同,可以在算法中做校正.

    比如水平和垂直分别做校正,最后和标准的样本比对,再进一步校正.