DLP4710模组里的usb转I2c和spi接口,我看图纸,应该是配置DLPC3439芯片的,好像也和msp430有连接。
请教有经验的朋友,这个usb口的一系列电路的详细功能是什么?能否在量产时去掉?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个USB接口主要的作用是给DLP4710评估模块做GUI调试用,量产时是不需要的。因为所有的控制都是通过前端AP发送I2C命令给DLPC3439实现的。
你好,不好意思,我是做硬件的,请问“前端AP”指的是什么?
还有,DLPC3439除了可以用两颗flash配置以外,还能用I2c和spi控制对吗?请问这三种配置方式有什么区别呢?
通常DLP4710应用于微型投影领域,比如视频显示。在系统的硬件架构上,DLPC3439芯片前端一般有视频处理IC或是独立的MCU,统称为前端AP。 DLPC3439外面的两颗SPI Flash芯片存储的是3439的固件,上电后3439读取flash以完成初始化。 前端如果要对DLPC3439显示做一些调整,例如亮度、显示通道等,都是通过前端的MCU发I2C命令给3439实现的。 SPI总线只做DLPC3439系统内部使用。
不好意思,再请问下,DLPC3439 外接的两颗SPI Flash芯片 怎么烧写固件啊?
还有,我打算用HDMI接口给投影机接,投影机上不打算加处理器,是不是就必须用msp430了呢?
PCB贴片以前先用烧录器把固件烧到flash里面,然后再贴片。若只做HDMI投影用,你可以参考TI官网上DLP4710评估模块的电路图。如果不需要调任何参数,MCU部分可以不用,但是在3439的固件里面要设置好,例如默认的输入信源,分辨率,电流大小等。