使用MSP430如何通过DPP2607給SPI读写Flash数据,求指教!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
读写Flash中关于
Led Total Power: 1W
AWB Temperature(℃): 35
Sequence Index(60Hz): 10
Sequence Index(50Hz): 2
Red DUTY(%): 27
R Led Peak Current(mA): 329
Green DUTY(%): 45
G Led Peak Current(mA): 325
Blue DUTY(%): 28
B Led Peak Current(mA): 329
White Lux: 78.4
White x: 0.293
White y: 0.3282
Black Lux: 0.0
Contrast: 1000
这里面的相关参数,谢谢!
这些基本都是光机本身的参数,不能通过SPI读到。请参考光机规格书,并对应设置。通常需要设的是LED的电流大小和sequence的序号。具体寄存器的值请参考programmer guide: http://www.ti.com.cn/cn/lit/ug/dlpu013/dlpu013.pdf