This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ON的时候是+17°,OFF的时候是-17°,系统关闭的时候是0°。
Measured relative to the plane formed by the overall micromirror array.
您好!
请参考DLP4710数据手册
Micromirror tilt direction is measured as in a typical polar coordinate system: measuring counter-clockwise from a 0° reference which is aligned with the +X Cartesian axis.
http://www.ti.com/cn/lit/ds/symlink/dlp4710.pdf
另外如下是DLP2010的光学设计,虽然有些不同但是可以作为参考。
http://www.ti.com/lit/an/dlpa074a/dlpa074a.pdf
谢谢