1. 通过Ti的GUI将参数Width in nm分别设置为7.02和12.87时,得到的光谱能量有明显差异。但是我们通过自己的代码调用Ti接口dlpspec_scan_write_configuration将参数值设为12.87时得到的光谱和7.02时完全一致。目前不清楚是参数设置失败还是其他原因?
2.利用Ti提供的源程序编译生成DLPNIRscanNanoGUI_1.1.9时失败。原因是DLP Spectrum Library的源码中只有.h和.a 文件,没有对应的.c(使用的编译环境为VS2010)。我们试图在官网找DLP Spectrum Library库的源代码,但是没有找到。Ti能否提供这个库源码(.c)或者DLPNIRscanNanoGUI_1.1.9中使用的这个库(.lib)?