我有一块DMD 9500,官方文档显示它是一款Type-A型DMD,工作波长为400-900nm。另一方面,TI也给出了DMD上康宁玻璃的光谱特性,可以看出Type-A型DMD在红外(>700nm)反射率降低,但是谱段测试到了2000nm。我是否可以在1550波段使用这一款DMD,尽管反射效率低一点?有没有因为红外波段而损坏DMD的风险?如果能使用,激光功率有什么要求(mW/cm^2)
链接为官方对于DMD的玻璃层的光谱特性。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我有一块DMD 9500,官方文档显示它是一款Type-A型DMD,工作波长为400-900nm。另一方面,TI也给出了DMD上康宁玻璃的光谱特性,可以看出Type-A型DMD在红外(>700nm)反射率降低,但是谱段测试到了2000nm。我是否可以在1550波段使用这一款DMD,尽管反射效率低一点?有没有因为红外波段而损坏DMD的风险?如果能使用,激光功率有什么要求(mW/cm^2)
链接为官方对于DMD的玻璃层的光谱特性。
DMD还有许多其他温度和要求, 才能保证可靠性.
http://www.ti.com/lit/ds/symlink/dlp9500.pdf
第14和15,16页.