This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

高光谱成像

Other Parts Discussed in Thread: DLP6500FYE, DLP9000, DLPNIRSCANEVM

DLP6500FYE和DLP9000设计用于宽频带可见光 (420nm – 700nm),有没有支持900~1700nm或700~2500nm的产品

  • 这两个DMD没有针对近红外优化的.可以使用:

    http://www.ti.com/tool/DLPNIRSCANEVM

      High Performance EVM MobileSensing EVM
    Key Features DLP NIRscan DLP NIRscan Nano
    Evaluation Module (EVM) Usage Benchtop/Portable Battery
    Featured Digital Micromirror Device DLP4500NIR DLP2010NIR
    Micromirror Array Size (pixels) 912 x 1140 854 x 480
    Micromirror Pixel Pitch (µm) 7.6 5.4
    Micromirror Tilt Angle (degrees) +/-12 +/-17
    EVM Wavelength Range 1350 - 2490 nm 900 - 1700 nm
    EVM Spectral Resolution 12 nm 10 nm
    EVM Max Scan Speed (kHz) 4 2.88
    EVM Signal-to-Noise Ratio 30,000:1
    (transmissive head)
    6,000:1
    (reflective head)