使用J11外触发信号接口,通过TRIG1_IN_CON接口给脉冲信号,信号源flash,设置出发模式为上升沿外触发,触发脉冲为10HZ 时,投影正常,触发脉冲超过10HZ时,投影异常,投影效果为多福图片叠加效果,这是什么问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用J11外触发信号接口,通过TRIG1_IN_CON接口给脉冲信号,信号源flash,设置出发模式为上升沿外触发,触发脉冲为10HZ 时,投影正常,触发脉冲超过10HZ时,投影异常,投影效果为多福图片叠加效果,这是什么问题?
您好!
Trigger Out2 Supply是输出信号trigger out2的电平,可以通过J15选择。
请参考原理图

您好!
感谢您使用TI的DLP产品。
能具体说明下操作的步骤吗?包括两种模式的配置是怎么样的?
谢谢!