您好,我现在使用的是DLP3000,官网上推荐使用DLPC300控制器,但是DLPC300没有指定的LED 驱动器IC,我该如何选择。同时我发现DLPC2607也能用来控制DLP3000,但是DLPC2607指定的LED驱动器IC,DLPA1000处于预发售状态,我想问问什么时候开放购买
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DLPC300主要使用在高级光控制, 比如结构光3D扫描, 机器视觉; 用于 3D 扫描的便携式点云生成参考设计(采用 DLP® 技术)
DLPC2607主要是微型投影; http://www.ti.com.cn/tool/cn/dlpc2607displayevm
所有这两个都有完整参考设计.
你们主要是什么应用?
你可以参考:
http://www.ti.com.cn/lsds/ti_zh/dlp/display-and-projection/pico-chipsets/pico-chipsets-overview.page
DLPC2607量产出来7年了,你可以选择新的系统.
如果你以前的系统没有使用DLPA100,现在如果替换部分器件,就不方便使用DLPA100, 因为DLPA100的驱动软件在DLPC2607中绑定在一起的.你得更新DLPC2607软件.工作量比较大.