在patter on the fly模式下
使用trigger out 2输出触发信号。
引脚4(supply)的强度正常,为3.3V
但是引脚5,即触发信号的峰峰值只有400mV左右,这是正常现象吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在patter on the fly模式下
使用trigger out 2输出触发信号。
引脚4(supply)的强度正常,为3.3V
但是引脚5,即触发信号的峰峰值只有400mV左右,这是正常现象吗?
S_TP18是500mV左右的方波,这个不对的.
你们是TI原装的lightcrafter9000电路板吗?
这个应该是3.3V方波的.输出频率是多少?
你设置一下,测量S_TP17输出,看幅度和波型.
如果DLPC900输出为0.5V的话,那这个脚就有可能已经打坏了.可以用于测试