我按照dlpu042.pdf安装,在安装OpenCV时遇到问题如下
CMake Warning (dev) at cmake/OpenCVUtils.cmake:203 (if):
Policy CMP0054 is not set: Only interpret if() arguments as variables or
keywords when unquoted. Run "cmake --help-policy CMP0054" for policy
details. Use the cmake_policy command to set the policy and suppress this
warning.
Quoted variables like "WIN32" will no longer be dereferenced when the
policy is set to NEW. Since the policy is not set the OLD behavior will be
used.
Call Stack (most recent call first):
CMakeLists.txt:136 (OCV_OPTION)
This warning is for project developers. Use -Wno-dev to suppress it.
我的系统是64位win10,Cmake 3.8.2
请问如何解决?